我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
How is the ATV61/ATV71 minimum speed setting adjusted?
Issue:
Adjust minimum speed on ATV61/ATV71.

Product line:
ATV61 ATV71

Environment:
All

Cause:
Modify speed reference

Resolution:
Go to the Simply Start or Settings menu.  Find parameter Low Speed and set to the desired minimum speed reference.