我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Is SoMove 2.6.3 compatible with Windows XP?
Issue
Getting error message when trying to connect with SoMove

Product Line:
All Altivar Drives

Environment:
SoMove

Cause:
SoMove is no longer compatible with Windows XP

Resolution:
The last version that was compatible with Windows XP was SoMove version 2.1.24 - we do not support any newer SoMove version on Windows XP