我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
My140CPU53414A is stuck in de-fragmentation mode. Is there any way to terminate this operation?
You will need to perform a power cycle on the CPU to terminate the operation.

This issue was fixed with the introduction of executive version 1.44E for CPUx341x. You should reflash the CPU to prevent this problem from re-appearing.

施耐德電機Taiwan

附件
q5rv144E.bin [400 KB]