搜尋常見問題
Proximity sensors XS - What plastic is the reference XSZE230 made of?
XSZE230 is a set of 2 plastic nuts M30 for cylindrical proximity sensors XS in dia 30mm, black colour. Material is PPS GF40. GF40 means 40% glass fiber reinforced. PPS means Polyphenylene Sulfide (Thermoplastic). Examples of PPS trade name = Ryton or Tecatron
發佈於:施耐德電機Taiwan
這是否有幫助?
探索更多