搜尋常見問題
Proximity sensors XS - What plastic is the reference XSZE208 made of?
XSZE208 is a set of 2 plastic nuts M8 for cylindrical proximity sensors XS in dia 8mm, black color. Material is PPS GF40. GF40 means 40% glass fiber reinforced. PPS stands for Polyphenylene Sulfide (Thermoplastic). Examples of PPS trade name = Ryton or Tecatron
發佈於:施耐德電機Taiwan
這是否有幫助?
探索更多