我們的品牌

Impact-Company-Logo-English Black-01-177x54

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Can the ATV320 be used for single phase input to run a three phase motor?

Article available in these languages: 西班牙文

Issue:
ATV320 single phase supply to a three phase motor

Product Line:
ATV320, Altivar 320 Machine drive

Environment:
All models

Cause:
Short circuit and HP ratings for VFDs supplied with single phase power.

Resolution:
Yes, the ATV320 is suitable for single phase supply to three phase motors.  See the information included in the Getting Started Annex, document NVE21777 attached to select.

施耐德電機Taiwan

附件
ATV320_Getting_Started_Annex_NVE21777_07.pdf [199.09 KB]
探索更多
系列:
探索更多
系列: