{}
搜尋常見問題
Which is the consumption of the BCPM main boards and the adapter boards?
The current draw of the BCPM main board with all four daughter boards is approximately 30mA.
The board is fused at 500mA so even in case of catastrophic failure it could not draw more than that.

施耐德電機Taiwan