{}
搜尋常見問題
Video: Battery Replacement for Back-UPS XS & RS LCD units.
Issue:
UPS indicates battery requires replacement.

Product Line:
  • BR1500LCD
  • BX1500LCD
  • BR1300LCD
  • BX1300LCD
  • BN1250LCD

Environment:
All Serial Numbers

Cause:
Failed selftest resulting in a need for battery replacement. UPS batteries require periodic replacement based on usage and operating environment.

Resolution:
The following video will provide details to removing and reconnecting the internal battery for the Back-UPS XS & RS LCD family of units.

施耐德電機Taiwan