{}
搜尋常見問題
Can you run a single phase motor with an ATS22 or ATS48 softstart?

Article available in these languages: 西班牙文

Issue:
Wanting to run a single phase motor with an ATS22 or ATS48 softstart.

Product Line:
Altistart 22, Altistart 48

Environment:
All

Cause:
Single phase

Resolution:
No, there is not a single phase option for these product lines.  ATS48 and ATS22 are designed to run 3-phase motors only.

施耐德電機Taiwan

探索更多
系列:
可能有幫助的文章
探索更多
系列: