我们今天能为您提供什么帮助?

Why does an ION8650C meter using a Cellular Modem drop connection randomly?

Issue
ION8650 meter drops Cellular Modem connection randomly

Product Line
ION8650 series meters

Environment
Cellular Modem connection

Cause
The meter is unable to retain its Cell Modem firewall information and drops its connection. Power cycling the meter would only resolve the issue for a few minutes.

Resolution
Upgrade ION8650 meter to firmware version 4.21.0 to resolve this issue.
ION8650 V4.21.0 can be downloaded from the Schneider Electric website.