我们今天能为您提供什么帮助?

Video: PlantStruxure PES: How to Configure Supervision Server Redundancy for Supervision Project in PES.

Goals and Symptoms

Video in this FAQ demonstrate how to configure Redundancy for Supervision Servers for Supervision Project in PES.

Facts and Changes

Steps mentioned in this Video shall be applicable for PES4.3 with Supervision Participant as Vijeo Citect.

Causes and Fixes

Once the Supervision project is created in PES, default it is being generated with Standalone Supervision Servers (IOServer, Alarm Server, Trend Server and Report Server). This Video demonstrate how to Configure Supervision Server Redundancy for Supervision Project in PES (Process Expert Solution). Prerequisites for this video demonstration is that user must have basic knowledge on PES Software, Supervision project has been configured for Standalone Server, in Build State and running on Network IP Address not on Loopback IP address.