{}
搜尋常見問題
PowerChute Network Shutdown v4.2 not communicating with iReasoning or MG-Soft when authentication protocol is set to SHA 512.
Issue:
PowerChute Network Shutdown v4.2 not communicating with iReasoning or MG-Soft when authentication protocol is set to SHA 512

Product Line:
PowerChute Network Shutdown version 4.2

Environment:
PowerChute Network Shutdown version 4.2 configured with NMS tool iReasoning or MG-Soft

Cause:
SNMPv3  profile created with SHA 512

Solution:
Create profile with SHA 256

施耐德電機Taiwan