我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What is the diameter and bend of radius of the cable VW3A1104R30?
Issue:
Needs to know the diameter and bend of radius of the VW3A1104R30 cable

Product Line:
ATV61/71

Environment:
VW3A1104R30


Cause:
N/A

Resolution:
The diameter of the cable is  5.6mm
The bending radius minimum is  50mm