我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What is the part number for the replacement connector (2 positions) of the TSXASY800 card?
Issue:
We need to order a replacement connector for the 2 positions green connector of the TSXASY800 premium card.

Product Line:
Premium, TSX, Modicon

Environment:
PLC

Resolution:
The connector on the TSXASY800 is not sold separate, we do not have a part number for it. However the customer can obtain the connector through Phoenix Contact. The manufacturer part number is 1757019. The part number alias is MSTB_2,5.

施耐德電機Taiwan

附件
1757019.pdf [230.88 KB]