我们今天能为您提供什么帮助?

How can I use a local language in Easergy P3?

By default, the device includes only English language but a local language package need to be installed and in some cases, also specific fonts need to be installed. In case you need the language package please contact Schneider technical support.

If a local language package is installed, you will be able to switch between English language and your local language. In case there is some text in language package which is not translated English text will be shown.