我们今天能为您提供什么帮助?

How can I connect and login to the FTP server in Easergy P3?

Use any FTP server program, e.g. FileZilla or you can also use Explorer. Write ftp:// and the IP address of device, e.g. ftp://10.158.45.40
User is fixed “easergy” and password is a setting, by default “config”