我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Which Unity version supports the 140CPU65160S
Issue
Which Unity version supports the 140CPU65160S

Product Line
Quantum 140CPU65160S

Environment
Windows 10

Resolution
Support for the 140CPU65160S is only available with Unity 7.
Any version later than Unity 7 does not support the Quantum 140CPU65160S