我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Video: How to configure the BMENOP0300 as a server
Issue
The goal of this video is to demonstrate how to configure a BMENOP0300 IEC61850 communications module as a Server.

Product Line
BMENOP0300

Environment
Windows 10, Unity

Resolution

SE USA Product Range URL
https://www.se.com/ww/en/product-range/61938-modicon-x80-i-os?Nrpp=10&Nr=AND(P_visibility:1,product.siteId:700002,OR(product.catalogId:catalog10007))&N=1329594164&No=20