搜尋常見問題
How to create mass trend logs and extended logs ?
To create mass trend logs and extended logs please follow the steps :-
Mass Creation of Interval Trend Logs
- Select all of the Values you wish to add the same type of Log to
- Right Click and select New>Trend
- Select the Log type and the settings you wish to use. Note that the log name will be the values name with either a prefix or suffix defined by the user
- Be sure to Select a useful folder location
- Click Next
- Set the Interval Settings
- Click Next
- Click Create
Mass Creation of Extended Trend Logs
- Select the group of Logs you wish to create Extended Trend Logs for
- Right Click and select New>Extended Trend Log
- Enter the desired settings. Just as above, the Extended log will use the Log' name plus either a prefix or suffix
- Be sure to Enter an appropriate Location. Use a folder on the ES if you wish these logs to show up on the Reports Server
- Click Next
- Configure the Extended Log as desired
- If you want all of these logs to show up in the Reports Server, set the "Include in reports" property to "True"
- Click Create
發佈於:施耐德電機Taiwan
探索更多
系列:
類別:
探索更多
系列:
類別: