我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Why can I not see Display Configuration Menu on ATV61 drives?
Issue:
Display Config under the Main Menu is not visible.

Product line:
Altivar 61, ATV61

Environment:
n/a

Cause:
n/a

Resolution:
To see the Display Config menu, the drive must be in Access Level of Advanced or Expert. You also have to have the Password function deactivated or turned off.