我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Is the ATV312 compatible with the VW3A1006 HMI Keypad?
Issue:
Is the VW3A1006 keypad compatible with the ATV312?

Product line:
ATV31, ATV312

Environment:
All models, All serial numbers.

Cause:
Firmware Compatibility

Resolution:
Yes, the VW3A1006, VW3A1007, and VW3A1101 keypads are compatible with the ATV312 series drives.