UMAC tool Version 2.x, the conversion of PUT_4X and GET_4X is not supported. The conversion results will return compile errors for each instance of these blocks.
To program a substitution for the blocks, a UINT array the size of the entire %MW available memory located to %MW1 can be created. You can then read from and write to the array using the array index and MOVE blocks.
*** UMAC v3.0 and up contains these blocks in the UMAC library and converts them properly ***
If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
發佈於:施耐德電機Taiwan