{}
搜尋常見問題
Is there a height difference between NetShelter cabinets with standard castors and heavy duty castors?
Issue:
A customer is asking about height difference caused by changing the castors.

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
There may be a height difference when the castors are changed.

Resolution:

There is no height difference on a cabinet if it uses standard castors or heavy duty castors. This includes AR3xxx, AR3xxx-717, AR3xxxSP.

施耐德電機Taiwan

探索更多
系列:
可能有幫助的文章
探索更多
系列: