{}
搜尋常見問題
Can the 20 and 28 pin 'Hardened' X80 IO modules use standard cables and terminal blocks?
Issue
Hardened terminal blocks are available for the 40 pin X80 'hardened' modules. Do the 20 and 28 pin 'hardened' X80 IO modules also have hardened connectors?

Product line
Modicon X80 I/O Modules

Resolution
The X80 40 Pin 'Hardened' modules include 'gold plating' and the standard connectors have 'tinned copper' connections. It is for this reason that 'Hardened' terminal blocks must be used with the 40 pin 'Hardened' modules. A difference of metals between connectors is not recommended as this causes galvanic corrosion over time. The issue does not exist with the 20 and 28 pin 'Hardened' X80 modules so standard terminal blocks and cable assemblies can be used.


If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

施耐德電機Taiwan

探索更多
系列:
可能有幫助的文章
探索更多
系列: