我们今天能为您提供什么帮助?

How to convert INT variable to ASCII characters in Vijeo Designer

1. Issue
How to convert INT variables to ASCII characters in Vijeo Designer.
2. Environment
Vijeo Designer V6.2[SPx]
3. Resolution
We can use scripts in Vijeo Designer to convert INT variables to ASCII characters. Below is an example to convert integer “65” to ASCII character.