{}

我們的品牌

Impact-Company-Logo-English Black-01-177x54

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
搜尋常見問題
PME2020 - An error occurred while executing command when running Diagnostics Tool
Issue

Issue 1:
When generating a PME Diagnostics, the Output analysis gives multiple errors like:
Executing command: Product and Device Information
An error occurred while executing command [Product and Device Information], see log for details.
Executing Command: SystemLog Events
An error occurred while executing command [SystemLog Events], see log for details.
Executing Command: AppMods Diagnostics
An error occurred while executing command [AppMods Diagnostics], see log for details.
Checking the Diagnostics log located at C:\Program Files (x86)\Schneider Electric\Power Monitoring Expert\Diagnostics Tool\Logs, the following error will be logged for all the failed steps:

[08.04.2020 13:56:49] Exception message: Input string was not in a correct format.
[08.04.2020 13:56:49] Stack Trace:    at System.Number.ParseSingle(String value, NumberStyles options, NumberFormatInfo numfmt)
at IONEnterpriseCommands.EnterpriseUtilities.GetConnectionString(String database)
at IONEnterpriseCommands.SystemLogCommand.Execute()
at DiagnosticsTool.DiagnosticsManager.ExecuteCommand(Object command)

Issue 2:
When generating a PME Diagnostics, the Output analysis gives multiple errors like:
Executing command: Product and Device Information
An error occurred while executing command [Product and Device Information], see log for details.

Checking the Diagnostics log located at C:\Program Files (x86)\Schneider Electric\Power Monitoring Expert\Diagnostics Tool\Logs, the following error will be logged for all the failed steps:

[08.04.2020 13:56:49] Exception message: "Exception has been thrown by the target of an invocation"

Product Line

Power Monitoring Expert 2020

Environment

Diagnostics Tool

Cause

When the Diagnostics tool is checking PME versions to determine how to connect to the databases, it was not parsing the 9.1 string properly into a number depending on the regional settings of the server ( some separator symbols may vary from culture to culture, like decimal separator for instance).

Resolution

1) Make sure the Diagnostic Tool is closed

2) Go to C:\Program Files (x86)\Schneider Electric\Power Monitoring Expert\Diagnostics Tool\Commands

3) Make a copy of IONEnterpriseCommands.dll (in a separate folder)

4) Replace it with the one attached

Additional Information
1) If the tool does not launch after applying the hotfix, make sure to unblock the new dll file.
- Right click > Properties> General tab > at the bottom > Unblock

2) There will be a new release of the tool that will include this hotfix.

施耐德電機Taiwan

附件
DiagnosticsTool-Release.5.1_Hotfix_20105.01.7z [40.28 KB]
探索更多
系列:
可能有幫助的文章
探索更多
系列: