我们今天能为您提供什么帮助?

NetBotz 750/755 "400 error" if not filling in identification fields fully

Issue:
NetBotz 750/755 "400 error" if not filling in identification fields fully

Product Line:
NetBotz

Environment:
NBRK0750
NBWL0755
Version 5.2.4 firmware and below

Cause:
If any of the identification fields are left blank when configuring Settings-->Identification on a NetBotz 750 or 755, a 400 error may appear

Resolution:
Be sure to fill each field with text and the error should not appear. It has also been seen where adding text, saving, then re-editing may allow for a blank field.

This issue is resolved in the NetBotz 5.3 release.