我们今天能为您提供什么帮助?

Changing NetBotz 750/755 hostname may result in change of device IP.

Issue:
Changing NetBotz 750/755 hostname may result in change of device IP.

Product Line:
NetBotz 5.x

Environment:
NBRK0750 NBWL0755/NBWL0756
DHCP


Cause:
Upon initial change of the NetBotz 750 / 755 hostname (under Settings-->System-->Network), the NetBotz unit when using DHCP may obtain a different IP address.

Resolution:
The only way to avoid this is by using a DHCP reservation or by statically assigning an IP to the NetBotz appliance.