Galaxy RPP “Fingersafe IP2X” NQ Panelboards
Issue:
The new Galaxy RPP has multiple panelboard options. One of them is the IP2X Fingersafe panelboard which greatly restricts exposure to live parts.
These panelboards use the standard Square D QOB breakers but require some adapters to make them fit and increase safety.
Product line:
GRPPIP2X84, GRPPIP2X89
Environment:
All models, all serial numbers
Cause:
Electrocution is one of the top causes of construction injury. The NQ panelboard reduces this risk by limiting exposure to live components.
Resolution:
To install standard Sq D QOB breakers into the Galaxy RPP with the NQ Panelboard, you will need an accessory jaw kit, and Fingersafe Barriers.
Parts:
| Catalog Number | Quantity per package | Description |
| QOFSBF12 | 12 | NQ IP2X Bus Finger Filler *3 |
| QOFSLALB12 | 12 | NQ IP2X QO(B) Lug Cover Low Amp |
| QOFSHALB12 | 12 | NQ IP2X QO(B) Lug Cover High Amp |
| QO1PJ15 | 15 | QOB Jaw Kit4 |
| QOBRT | 1 | QOB Breaker Removal Kit *4 |
| *3 Used only with Standard IP2X design | ||
| *4 Used only with Enhanced IP2X design | ||
References:
https://www.apc.com/shop/us/en/products/Galaxy-RPP-with-fingersafe-IP2X-panelboard-white/P-GRPPIP2X84
https://download.schneider-electric.com/files?p_File_Name=998-20824083_GMA-US_Galaxy+RPP+brochure_HR_WEB.pdf&p_Doc_Ref=GalaxyRPP_Brochure_EN&p_enDocType=Catalog
https://download.schneider-electric.com/files?p_enDocType=Brochure&p_File_Name=1640BR1701_NQ_FingerSafe1-2019.pdf&p_Doc_Ref=1640BR1701
發佈於: 施耐德電機Taiwan