我们今天能为您提供什么帮助?

How to use the PLC simulator

How to use the  PLC Simulator for EcoStruxure Control Expert.

The PLC Simulator is installed with EcoStruxure Control Expert.  It can be used to
test a Control Expert project during development.

This video will:
  • demonstrate how to create a Control Expert project and test it using the PLC simulator
  • demonstrate how to use the Control Panel for the PLC Simulator.
As a prerequisite, the user must be familiar with using EcoStruxure Control Expert and the M580 PLC.