Can I connect to and program my M580 through a CRA on a RIO drop?
Issue
Connect to M580 through CRA
Product Line
Modicon M580
Environment
EcoStruxure Control Expert
Resolution
Yes you can connect to an M580 through a CRA's service port. When connecting you wan to make sure you are connecting to the CPU's IP Address and not the CRA's.
發佈於: 施耐德電機Taiwan