我们今天能为您提供什么帮助?

What is the installation procedure as how to mount the TeSys Giga contactor without cable memory on a circuit breaker ?

TeSys Giga contactor can be installed directly to NSX circuit breakers, by aligning their terminal depth with dedicated flexible terminals extensions.

image.png
Note: TeSys Giga advanced version contactors are always delivered with cable memory kits pre-installed (LA9G310/ LA9G410●). The existing cable memory kit to be replaced with alternative flexible terminals extensions (LA9G311/ LA9G411●) when installing in alignment to NSX breaker main power terminals.