我们今天能为您提供什么帮助?

What topology options are supported on the VW3A3601 EtherCAT card for the ATV930 Drive?

Issue:

VW3A3601 EtherCAT topology options for the ATV930 Drive?

Product Line:

VW3A3601 EtherCAT option

Environment:

All

Cause:

Installation Topology

Resolution:

EtherCAT sheet 1