我们今天能为您提供什么帮助?

How do I create an admin badge for EVlink Pro AC ?

From the factory there is no admin badge recorded.
At the first power on of the charging station, the first badge tapped on the RFID reader is recorded as an admin badge. In this case the charging station will blink once. If the charging station does not blink it means there is another admin badge already recorded.
To create or erase another admin badge you need to use the eSetup app.
When you use a admin badge it is confirmed by a green smooth pulsing of the LED during 1 minute