我们今天能为您提供什么帮助?

What type of USB key can be use to update EVlink Pro AC firmware ?

You can use an USB key with a minimum capacity of 2 Go. The formats FAT32 or exFAT are compatible.
The USB key can have other folders but the Evlink Pro AC software need to be place directly at the root , not in a folder .
We recommend to analyze the USB key or USB storage device content with an anti-virus software before plugging it into the Charging Station USB port.