我们今天能为您提供什么帮助?

What are the settings on the EVlink Pro AC when an external Energy Meter is connected using RS485 Modbus protocol ?

9600 baud / Parity Even/stop bit:1 / Do not use the slave address 247.
Energy Meter references (MID): A9MEM2155, A9MEM3155.
Energy Meter References (non MID): A9MEM2150, A9MEM3150.