How do you set up Brake Logic Control on a ATV930 drive?
Issue:
Setting up Brake Logic Control on a ATV930 drive.
Product Line:
ATV930
Environment:
Brake Logic Control
Cause:
n/a
Resolution:
Go to 5.9 menu (Hoisting Functions)
Brake Logic Control- set to R2
Movement type- Hoisting or Traveling
Brake Contact- set to the corresponding Digital input
Brake Relay Feedback- set to the corresponding Digital input
Brake release Pulse – set to yes or no or 2IBR
Brake release Current-current you want the brake to release
Brake Release Time- suggest around .5 secs
Brake release Freq- Auto
Brake engage freq-Auto
Brake engage delay-.00 secs
Brake engage time-time to engage the brake- suggest around .5 secs
Engage at reversal- No (if you do not want the brakes to engage in reverse)
Jump at reversal-auto
Time to rstart-.00 secs
Current ramp time-.00 sec
發佈於: 施耐德電機Taiwan