What is the maximum number of Modbus TCP server connection supported by the TM3 bus coupler module TM3BCEIP?
Issue:
Maximum number of Modbus TCP server connection supported by the TM3 bus coupler module TM3BCEIP
Product Line:
EcoStruxure Machine Expert Basic, TM3
Resolution:
The maximum number of Modbus TCP server connection supported by the TM3BCEIP bus coupler module is 8
Maximum number of Modbus TCP server connection supported by the TM3 bus coupler module TM3BCEIP
Product Line:
EcoStruxure Machine Expert Basic, TM3
Resolution:
The maximum number of Modbus TCP server connection supported by the TM3BCEIP bus coupler module is 8
發佈於: 施耐德電機Taiwan
需要協助?
產品選型工具
快速輕鬆地為您的應用找到合適的產品和附件。
取得報價
立即線上提交您的銷售需求,專業團隊將主動聯繫您。
購買地點
輕鬆在您所在地區找到最近的施耐德電機經銷商。
支援中心
在同一位置找到滿足您所有需求的支援資源。