我们今天能为您提供什么帮助?

What causes a CPU fault on a ATV320 drive?

Issue:

Getting a CPU fault on a ATV320 drive.

Product Line:

ATV320

Environment:

CPU fault

Cause:

n/a

Resolution:

A CPU fault is an internal Main Control board CPU error. Try power cycling the drive, and if it does not reset ,then you will need to replace the drive.