我们今天能为您提供什么帮助?

How to configure the Harmony Edge Box HMISTM6BOXIOT to send data in SQL Database?

The goal of this FAQ is to share some complementary documentation and demo project to connect HMISTM6BOXIOT to SQL Database.

This article, demo and manual are applicable for HMISTM6BOXIOT with EcoStruxure Machine SCADA Expert 2020 SP2 (minimum).

The Demo project: https://schneiderelectric.sharepoint.com/:u:/s/BoxSupportL3Group/EQPSIH_zxHlCudO-C2R8jlkBnR1-RkDpYOmoeVe_1MLmwg?e=QwPXWa
The Demo Setup Guide: https://schneiderelectric.sharepoint.com/:b:/s/BoxSupportL3Group/EQpjjCwejHNIi7AH-1Cj2HoBryrcCS4Jz22sOOPYJZF1uA?e=WTmZYu