我们今天能为您提供什么帮助?

What is the insulation resistance and dielectric strength test for BMXFTA150?

Issue
What is the insulation resistance and dielectric strength test for BMXFTA150?

Product line
X80 I/O Modules SUB-D Connector

Environment
BMXFTA150

Resolution
The insulation resistance test is 20 ohms per kilometer and the dielectric strength is 1000 VDC.