我们今天能为您提供什么帮助?

What are the NTP restrictions on BMENUA0100 firmware version 2.01?

NTP protocol on BMENUA0100 won’t be available to be configured in the “forward services” in the webpage
BMENUA0100 used as a NTP server will restrict its answers only to a NTP client on its own subnet
BMENUA0100 used as NTP client should only be used on the same subnet as the NTP server BMENUA0100 version 2.01
Environment
Windows, EADM