我们今天能为您提供什么帮助?

What is the part number for the FT-21 Switchboard case for the ION8650 meter?

Issue
Looking for the part number for the switchboard case only.

Product Line
ION8650

Resolution
ION8650 form factor ordering options 4 and 7 already come with the FT-21 switchboard case and it does not need to be ordered separately if ordering either of these two options.

If you need the FT-21 switchboard case only, the part number is FR86XXCSESWB

This is the part number for the FT-21 switchboard case with breakout panel.

There is currently not a part number for the FT-21 switchboard case with breakout cable.