M580 counter modules
Issue
Using the Modicon M580 family I would like to get input from a 5VDC incremental encoder to track position. Is there an input module I can use for this? If not, what other options do I have? If I convert the 5VDC to 24VDC is there a input module that can track a 24VDC quadrature input?
Product Line
Modicon M580, Modicon X80
Resolution
We do not have a 5VDC module for an incremental encoder. If you have a 24VDC signal, we do offer the BMXEHC0200 which supports quadrature.
Here is a link to a YouTube video on the subject. https://www.youtube.com/watch?v=cNf5adjfBFE
發佈於: 施耐德電機Taiwan