我们今天能为您提供什么帮助?

Is it possible to change the EcoStruxure OPC UA Server Expert client session timeout value?

Issue:
EcoStruxure OPC UA Server Expert  client session timeout


Product Line:
EcoStruxure OPC UA Server Expert


Resolution:
No. Is is not possible to change the EcoStruxure OPC UA Server Expert Client session timeout value. The default value is 600s or 10 min.