我们今天能为您提供什么帮助?

ATV212 - Getting Err1 faults

Issue:

ATV212 drive getting Err 1 faults

Product Line:

ATV212

Environment:

Err 1 faults

Cause:

n/a

Resolution:

Err 1 faults on the ATV212 indicates that the scaling parameters for either VIA or VIB are not set correctly. Please check parameters F201- F204 (for VIA) or F210 to F213 (for VIB).