我们今天能为您提供什么帮助?

Is there a RAMP function block in EcoStruxure Control Expert?


Issue:
RAMP function block in EcoStruxure Control Expert


Product Line:
EcoStruxure Control Expert


Resolution:
Yes. You can use either the RAMP function block or the FGEN function block with a value of of 2 for the func_no element of the FGEN_Para structure


ramp




fgen