我们今天能为您提供什么帮助?

How can I select ATV32 under STBNIP2212 SV4.0

Issue:

How can I select ATV32 under STBNIP2212 SV4.0 ?

Product Line:

STB

Environment:

Advantys

Resolution:

User could install Advantys 12.3 and ATV32 device under enhanced canopen catalog could be selected when STBNIP/NIC2212 with SV4.XX are deployed.

demo