我们今天能为您提供什么帮助?

What is the heat dissipated by the UPS Galaxy 5500.

The value depends on the KW rating of the UPS.
This information is found in the Installation manual page 13: attachedG5500 heat dissipation

施耐德電機Taiwan

附件
MPOD-95HEHV_R3_EN (1).pdf [7.09 MB]