我们今天能为您提供什么帮助?

What is the maximum number of TCP/IP connections for the BMEP586040S

The maximum number of simultaneous TCP/IP connections on the BMEP586040S is the same as on the BMEP586040.  The following table shows the maximum number of connections for the M580 CPU's.

connections